Search results for: 高效的IdentityIQ-Engineer PDF和資格考試的領先材料供應商和最佳的IdentityIQ-Engineer 真題材料 🍾 在➽ www.newdumpspdf.com 🢪搜索最新的☀ IdentityIQ-Engineer ️☀️題庫IdentityIQ-Engineer認證考試
USB Interoperability Testing for Intel® RealSense™ Cameras
March 16, 2021This document captures the testing equipment and topology that is used when testing the Intel® RealSense™ Cameras for USB interoperability. The equipment, topology, and testing are done in accordance with the specification from usb.org.
Read MoreAethon: Industry-Changing Mobile Delivery Solutions
May 18, 2020Case Study: Aethon Download How Intel® RealSense™ depth sensing technology is helping Aethon create industry-changing mobile delivery solutions. Challenge Solution Results Challenge Healthcare, manufacturing, and hospitality industries face a costly challenge— moving things from place to place efficiently. Many mobile delivery robots require multiple sensors and complicated programming, and this means a higher bill of materials…
Read MoreDepth Camera D405
March 11, 2022Intel® RealSense™ Depth Camera D405 Buy Intel® RealSense™ D405. See the world up close. The Intel® RealSense™ Depth Camera D405 is a short-range stereo camera providing sub-millimeter accuracy for your close-range computer vision needs. Buy Play Video Small features, high impact Sub-millimeter accuracyThe D405 operates at an ideal range of 7 cm to 50 cm with minimum…
Read MoreDepth camera and edge ai
August 21, 2019Intel® RealSense™ Depth Cameras and Intel® Neural Compute Stick 2 Intel® RealSense™ Depth Cameras and Intel® NCS2 Depth Sensing + Edge AI Depth sensing meets plug‑and‑play AI at the edge inferencing with Intel® RealSense™ stereo depth cameras bundled with the Intel® Neural Compute Stick 2. Under the hood Get to know our best‑in‑class depth cameras and AI development kit in detail. View tech specs → Powered by…
Read MoreDepth Camera D415
January 7, 2019Intel® RealSense™ Depth Camera D415 Buy Depth Camera D415 The Intel® RealSense™ D415 has a standard field of view well suited for high accuracy applications such as 3D scanning. With a rolling shutter on the depth sensor, the D415 offers our highest depth quality per degree. Precision and Accuracy When accuracy is the most important factor for your solution, the D415 is the perfect choice.…
Read MoreDepth Camera D455
June 5, 2020Intel® RealSense™ Depth Camera D455 Buy Twice the range. Better performance. Introducing the latest addition to the family, the Intel® RealSense™ Depth Camera D455. The D455 is the fourth in the D400 series, designed from feedback and knowledge gained from over 10 years of stereo camera development. Buy Introducing the latest addition to the family, the Intel® RealSense™ Depth Camera D455. The D455…
Read MoreANYbotics
April 14, 2022Case Study: Robotics Download Intel RealSense helps autonomous mobile robots map facilities, avoid obstacles, climb stairs, and navigate to dynamic docking stations Challenge Solution Results Challenge Industrial sites are complex environments. Monitoring the condition of equipment and infrastructure is mandatory. But industrial inspections are often tedious, error-prone tasks that expose humans to hazardous environments. Solution…
Read More