Retail automation using Robotics with Simbe Robotics and Tally.

Skip to content
Simbe

Simbe’s Real-Time Store Intelligence™ Platform Powered by Intel RealSense Depth Cameras

Harnessing Computer Vision, AI, and Robotics to Revolutionize Retail Inventory Management.

Simbe and Intel RealSense
Simbe and Intel RealSense

Challenge

One of the biggest gaps in retail today is visibility into the store interior. Retailers know when inventory arrives and when it sells, but what happens in between is often a mystery. Common problems like out-of-stock items, pricing errors, and missed promotions can leave retailers scrambling.

Solution

As the most advanced autonomous inventory robot on the market, Tally helps retailers gain the visibility they need to manage inventory more efficiently and improve their bottom lines. Intel RealSense Depth Cameras D435 and D415 empower Tally to map shelves, monitor inventory, and confirm pricing accuracy while navigating safely and efficiently through retail environments.

Results

Tally audits up to 30,000 items per hour, spotting out-of-stock items, misplaced products, and pricing discrepancies. Stores using Tally see a 2% increase in sales, 98% on-shelf availability, and save 50 hours a week—allowing associates to focus more on customer service. With Tally’s help, retailers cut out-of-stock rates by 60% and see higher shopper satisfaction.

Bringing Intelligence to the Aisles

Store interiors continue to be one of the biggest blind spots in retail. Without accurate and real-time shelf data, stores struggle with fundamental issues like out-of-stock items, incorrect pricing and promotions. Each year these issues cost retailers billions  in lost revenue and customer satisfaction. This is where Simbe’s Tally comes in, transforming the shelf into a source of actionable insights.

Digitizing Store Operations with Autonomous Intelligence

Tally, the first autonomous item-scanning robot for retail, delivers the clarity retailers need into the store environment. Tally utilizes sophisticated AI and computer vision to monitor product location, inventory levels, and pricing with advanced algorithms and computer vision. By scanning shelves multiple times a day, Tally replaces outdated planograms with a real-time “realogram,” helping retailers operate with greater efficiency and accuracy.

Designed to Work Seamlessly in Any Store

Tally is easy to deploy and requires only Wi-Fi and a power outlet. While moving autonomously through aisles, it captures data while coexisting with shoppers and store associates. Tally's compact form and multi-camera navigation allow it to operate in the most crowded environments without concern.

Designed to be shy and unobtrusive, Tally can operate alongside shoppers and store associates during regular business hours.

Tally pays for itself within 30 days at a new store, with an average 20% reduction in out of stock items and improved customer satisfaction.

Tally can audit around 10,000 items in 30 minutes, identifying issues such as out-of-stock items, misplaced merchandise, incorrect price tags, outdated promo tags and more.

The Role of SDK 2.0 in Accelerating Innovation

Simbe leverages Intel RealSense SDK 2.0 to integrate and fine-tune depth sensing capabilities within Tally’s system. Our robust software toolkit allows for rapid prototyping, seamless customization, and precise control over camera behavior—helping Simbe stay ahead of evolving retail demands with speed and confidence.

The heart of the solution

To fuel its cutting-edge shelf-scanning abilities, Simbe chose Intel RealSense Depth Cameras D415 and D435. They detect  gaps between products and shelves, providing high-resolution depth data necessary for accurate inventory mapping. Compact size and low power consumption make D435 and D415 depth cameras perfect for continuous use in large retail environments.

D435

Depth Camera D435
Field of View

FOV 87° × 58°

Ideal range

Ideal Range 0.3 m to 3 m

Shutter type

Global Shutter

D415

Depth Camera D415
Field of View

FOV 65° × 40°

Ideal range

Ideal Range 0.5 m to 3 m

Shutter type

Rolling Shutter

brad-bogolea

Brad Bogolea

Simbe CEO

Intel RealSense depth cameras offer a seamless out-of-the-box experience with one of the most reliable multi-camera systems on the market, an important factor in our decision to work with Intel RealSense.

What's next?

Learn how RightHand Robotics is using Intel® RealSense™ computer vision technology to revolutionize automated warehouse order fulfillment.

Robotics overview

See how Intel® RealSense™ cameras can revolutionize the robotics industry with the latest in depth‑sensing technology.

Ready to talk to sales?
Contact Sales
Scroll To Top